i.MX8M mini TMU SW calibration code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M mini TMU SW calibration code

ソリューションへジャンプ
2,170件の閲覧回数
Tori-san
Contributor III
Hello, Is imx8mm_thermal.c the code to perform SW calibration? Current version is "imx_5.4.70_2.3.0", but are there any plans to update it for TMU SW calibration?
0 件の賞賛
返信
1 解決策
2,162件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  Generally the calibration points are measured during the manufacturing testing,
and are programmed in the fuse registers - no need for customers to implement
the calibration.

Regards,
Yuri.

元の投稿で解決策を見る

2 返答(返信)
2,163件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

  Generally the calibration points are measured during the manufacturing testing,
and are programmed in the fuse registers - no need for customers to implement
the calibration.

Regards,
Yuri.

2,148件の閲覧回数
Tori-san
Contributor III
Hi Yuri, Thank you for your reply. I interpret that I don't need to calibrate with the default setting. However, if more accurate calibration is required, it should be implemented in the driver(imx8mm_thermal.c) using the equation desribed in RM. Best regards, Tori-san.