IMX6SLEVK + IMXEBOOKDC4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SLEVK + IMXEBOOKDC4

1,242 Views
raadel
Contributor I

What would be the most recent and known good Linux version (Yocto Project User's Guide version), distribution and image configuration to be used with IMX6SLEVK and IMXEBOOKDC4 EPDC addon?

Previously, I tried according to IMXLXYOCTOUG (Rev. L4.9.88_2.0.0-ga, 05/2018) using:

DISTRO=fsl-imx-fb MACHINE=imx6slevk source fsl-setup-release.sh -b build-fb

echo "UBOOT_CONFIG = \"epdc\"" >> conf/local.conf

bitbake fsl-image-validation-imx

The compiled image included EPDC test applications, but the framebuffer device for EPDC (/dev/fb2) was always incorrectly configured for 800x1200 resolution:

root@imx6slevk:/unit_tests/Display# ./mxc_epdc_fb_test.out

---- Running < ./mxc_epdc_fb_test.out > test ----

Opened EPDC fb device /dev/fb2
Set the background to 16-bpp
screen_info.xres_virtual = 800
screen_info.yres_virtual = 1280
screen_info.bits_per_pixel = 16

Now I tried to use the more recent version of the Yocto Project User's Guide (Rev. L5.4.70_2.3.0 — 31 December 2020), but I'm not sure what distro and image configuration to use for EPDC on IMX6SLEVK + IMXEBOOKDC4.

 

0 Kudos
Reply
1 Reply

1,217 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi raadel,

 

You can use the DISTRO=fsl-imx-fb MACHINE=imx6slevk source imx-setup-release.sh -b build-fb of course adding the epdc and for change the resolution you can use this on U-boot:

 setenv bootargs console=${console},${baudrate} root=${mmcroot} epdc video=mxcepdcfb:ED060KG2C1,bpp=16 max17135:pass=2,vcom=-2560000

 

Regards,

Israel.

0 Kudos
Reply