i.MX6DQ OE and OC assert/negate timing in async mode.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6DQ OE and OC assert/negate timing in async mode.

跳至解决方案
1,331 次查看
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6DQ EIM.

According to the figures in chapter 22.8 of IMX6DQRM Rev.3, OE and OC signal is asserted/negated at the rising edge of EIM CLK in asynchronous mode.

On the other hand, in IMX6DQCEC Rev.4, OE and OC signal is asserted/negated at the falling edge of INT_CLK.

Which is correct?

Best Regards,

Satoshi Shimoda

标签 (4)
标记 (1)
0 项奖励
回复
1 解答
1,125 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

correct is rising edge of EIM CLK, also datasheet pictures show

timing references to rising edge

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,126 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

correct is rising edge of EIM CLK, also datasheet pictures show

timing references to rising edge

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复