i.MX6DQ OE and OC assert/negate timing in async mode.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DQ OE and OC assert/negate timing in async mode.

ソリューションへジャンプ
1,355件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6DQ EIM.

According to the figures in chapter 22.8 of IMX6DQRM Rev.3, OE and OC signal is asserted/negated at the rising edge of EIM CLK in asynchronous mode.

On the other hand, in IMX6DQCEC Rev.4, OE and OC signal is asserted/negated at the falling edge of INT_CLK.

Which is correct?

Best Regards,

Satoshi Shimoda

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 解決策
1,149件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

correct is rising edge of EIM CLK, also datasheet pictures show

timing references to rising edge

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,150件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

correct is rising edge of EIM CLK, also datasheet pictures show

timing references to rising edge

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信