i.MX6 Boot device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,268件の閲覧回数
vishakh
Contributor III

Hi,

We are using i.MX6Q processor.

Does this support Boot from USB mass storage device?

Thanks and Regards,

Vishakh

ラベル(1)
0 件の賞賛
返信
1 解決策
2,088件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 bootROM does not support USB mass storage device.

But the bootROM supports special USB boot mode, that may be used

to load and run an application, using a host PC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,089件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 bootROM does not support USB mass storage device.

But the bootROM supports special USB boot mode, that may be used

to load and run an application, using a host PC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,088件の閲覧回数
saurabh_patel
NXP Pro Support
NXP Pro Support
0 件の賞賛
返信