i.MX6 Boot device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 Boot device

跳至解决方案
2,232 次查看
vishakh
Contributor III

Hi,

We are using i.MX6Q processor.

Does this support Boot from USB mass storage device?

Thanks and Regards,

Vishakh

标签 (1)
0 项奖励
回复
1 解答
2,052 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 bootROM does not support USB mass storage device.

But the bootROM supports special USB boot mode, that may be used

to load and run an application, using a host PC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,053 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 bootROM does not support USB mass storage device.

But the bootROM supports special USB boot mode, that may be used

to load and run an application, using a host PC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,052 次查看
saurabh_patel
NXP Pro Support
NXP Pro Support
0 项奖励
回复