i.MX6 Boot device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Boot device

Jump to solution
2,294 Views
vishakh
Contributor III

Hi,

We are using i.MX6Q processor.

Does this support Boot from USB mass storage device?

Thanks and Regards,

Vishakh

Labels (1)
0 Kudos
Reply
1 Solution
2,114 Views
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 bootROM does not support USB mass storage device.

But the bootROM supports special USB boot mode, that may be used

to load and run an application, using a host PC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,115 Views
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 bootROM does not support USB mass storage device.

But the bootROM supports special USB boot mode, that may be used

to load and run an application, using a host PC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,114 Views
saurabh_patel
NXP Pro Support
NXP Pro Support
0 Kudos
Reply