i.MX 8M Support for CBT (Command Bus Training)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX 8M Support for CBT (Command Bus Training)

跳至解决方案
3,130 次查看
koethe
Contributor II

Hello,

other i.MX 8/8X does support CBT (Command Bus Training) i.MX 8/8X Family DDR Tools Release, Details see MX8QM_B0_LPDDR4_RPA_1.6GHz_v20.xlsx.

Question: Is there an Option to perform CBT on a i.MX 8M ?

标签 (1)
0 项奖励
回复
1 解答
3,043 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

i.MX8M has different PHY version and CBT is performed automatically by the DDR PHY

during DRAM initialization. For i.MX8 training is performed as part of initialization script.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
3,044 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

i.MX8M has different PHY version and CBT is performed automatically by the DDR PHY

during DRAM initialization. For i.MX8 training is performed as part of initialization script.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,043 次查看
smithclarkson00
Contributor I

i had the same question....https://vidmateapp.win.

0 项奖励
回复