i.MX 8M Support for CBT (Command Bus Training)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8M Support for CBT (Command Bus Training)

ソリューションへジャンプ
3,155件の閲覧回数
koethe
Contributor II

Hello,

other i.MX 8/8X does support CBT (Command Bus Training) i.MX 8/8X Family DDR Tools Release, Details see MX8QM_B0_LPDDR4_RPA_1.6GHz_v20.xlsx.

Question: Is there an Option to perform CBT on a i.MX 8M ?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,068件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

i.MX8M has different PHY version and CBT is performed automatically by the DDR PHY

during DRAM initialization. For i.MX8 training is performed as part of initialization script.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
3,069件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

i.MX8M has different PHY version and CBT is performed automatically by the DDR PHY

during DRAM initialization. For i.MX8 training is performed as part of initialization script.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,068件の閲覧回数
smithclarkson00
Contributor I

i had the same question....https://vidmateapp.win.

0 件の賞賛
返信