i.MX 8M Support for CBT (Command Bus Training)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Support for CBT (Command Bus Training)

Jump to solution
3,127 Views
koethe
Contributor II

Hello,

other i.MX 8/8X does support CBT (Command Bus Training) i.MX 8/8X Family DDR Tools Release, Details see MX8QM_B0_LPDDR4_RPA_1.6GHz_v20.xlsx.

Question: Is there an Option to perform CBT on a i.MX 8M ?

Labels (1)
0 Kudos
Reply
1 Solution
3,040 Views
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

i.MX8M has different PHY version and CBT is performed automatically by the DDR PHY

during DRAM initialization. For i.MX8 training is performed as part of initialization script.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
3,041 Views
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

i.MX8M has different PHY version and CBT is performed automatically by the DDR PHY

during DRAM initialization. For i.MX8 training is performed as part of initialization script.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,040 Views
smithclarkson00
Contributor I

i had the same question....https://vidmateapp.win.

0 Kudos
Reply