does imx7d support MII interface ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

does imx7d support MII interface ?

ソリューションへジャンプ
1,725件の閲覧回数
jiangyaqiang
Senior Contributor I

Hi anyone:

I found in RM of imx7d, some MII interface PIN is missing or wrong. 

example:

pastedImage_1.png

TX_CLK should be use as input ,but in RM it's ouput.

and there is no ENET1_TX_EN pin. 

RGMII_TX_CTL is similar to TX_EN, but it used for RGMII only

pastedImage_2.png

Does anyone know the detail of pin assignment for MII interface?

MII interface should contains the following pins:

TXD[0:3] TX_ER TX_CLK/TXC  TX_EN  RXD[0:3] RX_CLK RX RX_XDV COL CRS
ラベル(3)
0 件の賞賛
返信
1 解決策
1,599件の閲覧回数
art
NXP Employee
NXP Employee

1. There is the typo in the manual regarding the ENETx_TX_CLK signal. Actually, it is input in the MII mode.

2. There is the typo in the manual regarding the RGMIIx_TX_CTL signal. Actually, in MII mode it operates as ENETx_TX_EN.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,600件の閲覧回数
art
NXP Employee
NXP Employee

1. There is the typo in the manual regarding the ENETx_TX_CLK signal. Actually, it is input in the MII mode.

2. There is the typo in the manual regarding the RGMIIx_TX_CTL signal. Actually, in MII mode it operates as ENETx_TX_EN.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信