delay unit for DQ setting in MMDC register for i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

delay unit for DQ setting in MMDC register for i.MX6

1,156 次查看
ko-hey
Senior Contributor II

Hi all,

 

I have question about delay unit in MMDC register.

Could you tell me the delay unit period ?

 

According to the description of MMDCx_MPRDDQBY0DL in IMX6DQRM, it shows the delay as below.

 

010         Add dq0 delay of 2 delay units.

011         Add dq0 delay of 3 delay units.

 

Does above period is same as following thread ?

https://community.nxp.com/message/483747

 

The thread said that 1 delay unit is 2-3[ps].

Does the delay unit which is described in MMDCx_MPRDDQBY0DL same ?

 

 

Ko-hey

 

标签 (2)
0 项奖励
回复
1 回复

1,078 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  typical delays are  on the order of picoseconds.

“Q&A: Delay units in SDCLKx_DEL of MMDCx_MPSDCTRL register”

 

https://community.nxp.com/docs/DOC-95580

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 项奖励
回复