apt-get not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

apt-get not working

8,362 次查看
ajayvenkatakris
Contributor II

I can not install any package as the apt-get command does not work in my sabre auto imx6qsolo. How do I install packages?

标记 (2)
11 回复数

6,190 次查看
Carlos_Musich
NXP Employee
NXP Employee

You may find this interesting

How do I - Yocto Project 

Regards,

Carlos

6,190 次查看
ajayvenkatakris
Contributor II

Hi,

   Even though I managed to get apt-get, a sources file is missing and apt-get install does not work. 

0 项奖励
回复

6,190 次查看
radimkratochvil
NXP Employee
NXP Employee

Hi Ajay,

what Linux you are using? Is that a Yocto or you have different distribution?

Radim.

0 项奖励
回复

6,190 次查看
ajayvenkatakris
Contributor II

Yes it yocto only. Can you specify the link of the OS which I can flash in the sabre auto board using Mfgtools, something which supports most linux commands?

0 项奖励
回复

6,190 次查看
radimkratochvil
NXP Employee
NXP Employee

At this moment, there is only prepared Android and Yocto. If you want to build your own Ubuntu you can use this tutorial https://community.nxp.com/docs/DOC-330147 

Radim.

0 项奖励
回复

6,190 次查看
ajayvenkatakris
Contributor II

Hi,

    The link you provided for building Ubuntu rootfs does not work due to a faulty link in the steps provided.

https://releases.linaro.org/14.09/components/toolchain/binaries/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux.tar.xz.

This link does not take me to the required page.

0 项奖励
回复

6,190 次查看
radimkratochvil
NXP Employee
NXP Employee
0 项奖励
回复

6,190 次查看
ajayvenkatakris
Contributor II

Hi, thank you for the solution. One more thing I wanted to know is that I have an SD with Raspbian OS in it. Can it be run by the imx6 board?

0 项奖励
回复

6,190 次查看
radimkratochvil
NXP Employee
NXP Employee

No, it can't.

Radim.

0 项奖励
回复

6,190 次查看
ajayvenkatakris
Contributor II

I have tried the link you suggested but I am getting a lot of errors. Where can I find a prepared yocto, that supports commands like apt-get for my sabre-auto board?

0 项奖励
回复

6,190 次查看
radimkratochvil
NXP Employee
NXP Employee

Yocto don't have packages, so when you have it on the SD card, you have to build everything extra. Only way to get packages to Yocto image is when you are building the image. i.MX Yocto Project: How do I add an existing package to an image? 

Radim.

0 项奖励
回复