apt-get not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

apt-get not working

10,630件の閲覧回数
ajayvenkatakris
Contributor II

I can not install any package as the apt-get command does not work in my sabre auto imx6qsolo. How do I install packages?

ラベル(4)
タグ(2)
11 返答(返信)

8,458件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

You may find this interesting

How do I - Yocto Project 

Regards,

Carlos

8,458件の閲覧回数
ajayvenkatakris
Contributor II

Hi,

   Even though I managed to get apt-get, a sources file is missing and apt-get install does not work. 

0 件の賞賛
返信

8,458件の閲覧回数
radimkratochvil
NXP Employee
NXP Employee

Hi Ajay,

what Linux you are using? Is that a Yocto or you have different distribution?

Radim.

0 件の賞賛
返信

8,458件の閲覧回数
ajayvenkatakris
Contributor II

Yes it yocto only. Can you specify the link of the OS which I can flash in the sabre auto board using Mfgtools, something which supports most linux commands?

0 件の賞賛
返信

8,458件の閲覧回数
radimkratochvil
NXP Employee
NXP Employee

At this moment, there is only prepared Android and Yocto. If you want to build your own Ubuntu you can use this tutorial https://community.nxp.com/docs/DOC-330147 

Radim.

0 件の賞賛
返信

8,458件の閲覧回数
ajayvenkatakris
Contributor II

Hi,

    The link you provided for building Ubuntu rootfs does not work due to a faulty link in the steps provided.

https://releases.linaro.org/14.09/components/toolchain/binaries/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux.tar.xz.

This link does not take me to the required page.

0 件の賞賛
返信

8,458件の閲覧回数
radimkratochvil
NXP Employee
NXP Employee
0 件の賞賛
返信

8,458件の閲覧回数
ajayvenkatakris
Contributor II

Hi, thank you for the solution. One more thing I wanted to know is that I have an SD with Raspbian OS in it. Can it be run by the imx6 board?

0 件の賞賛
返信

8,458件の閲覧回数
radimkratochvil
NXP Employee
NXP Employee

No, it can't.

Radim.

0 件の賞賛
返信

8,458件の閲覧回数
ajayvenkatakris
Contributor II

I have tried the link you suggested but I am getting a lot of errors. Where can I find a prepared yocto, that supports commands like apt-get for my sabre-auto board?

0 件の賞賛
返信

8,458件の閲覧回数
radimkratochvil
NXP Employee
NXP Employee

Yocto don't have packages, so when you have it on the SD card, you have to build everything extra. Only way to get packages to Yocto image is when you are building the image. i.MX Yocto Project: How do I add an existing package to an image? 

Radim.

0 件の賞賛
返信