android M6 audio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,156件の閲覧回数
imx-talent
Contributor I

平台:imx6dl-sabresd 系统: android 6.0

      遇到问题如下:

      一、播放*.wav出错

01-01 00:34:38.504   510   642 I ActivityManager: START u0 {act=android.intent.action.MAIN cat=[android.intent.category.LAUNCHER] flg=0x10200000 cmp=com.android.music/.MusicBrowserActivity (has extras)} from uid 10010 on display 0

01-01 00:34:38.692   510  1081 I ActivityManager: START u0 {act=android.intent.action.PICK dat= typ=vnd.android.cursor.dir/artistalbum flg=0x4000000 cmp=com.android.music/.ArtistAlbumBrowserActivity (has extras)} from uid 10042 on display 0

01-01 00:34:38.834   580   580 V PhoneStatusBar: setLightsOn(true)

01-01 00:34:39.359   212  3954 D NuPlayerDriver: notifyListener_l(0xb6056d80), (1, 0, 0)

01-01 00:34:39.360   934   934 D MediaPlayer: setSubtitleAnchor in MediaPlayer

01-01 00:34:39.370   212   212 D NuPlayerDriver: seekTo(0xb6056d80) 0 ms

01-01 00:34:39.370   212   212 D NuPlayerDriver: notifyListener_l(0xb6056d80), (7, 0, 0)

01-01 00:34:39.370   212  3954 I GenericSource: start

01-01 00:34:39.372   934   934 D MediaPlaybackService: restored queue, currently at position 0/260754 (requested 0)

01-01 00:34:39.373  1119  1119 V MusicFXControlPanelReceiver: onReceive

01-01 00:34:39.374  1119  1119 V MusicFXControlPanelReceiver: Action: android.media.action.OPEN_AUDIO_EFFECT_CONTROL_SESSION

01-01 00:34:39.374  1119  1119 V MusicFXControlPanelReceiver: Package name: com.android.music

01-01 00:34:39.374  1119  1119 V MusicFXControlPanelReceiver: Audio session: 11

01-01 00:34:39.374  1119  1119 V MusicFXControlPanelEffect: openSession(android.app.ReceiverRestrictedContext@5b72e54, com.android.music, 11)

01-01 00:34:39.403   212  3954 D NuPlayerDriver: notifyListener_l(0xb6056d80), (4, 0, 0)

01-01 00:34:39.421   212  3959 E OMXNodeInstance: setConfig(21:google.raw.decoder, ConfigPriority(0x6f800002)) ERROR: Undefined(0x80001001)

01-01 00:34:39.421   212  3959 I ACodec  : codec does not support config priority (err -2147483648)

01-01 00:34:39.423   212  3959 I MediaCodec: MediaCodec will operate in async mode

01-01 00:34:39.428   212  3957 W APM::AudioPolicyManager: getOutput() could not find output for stream 3, samplingRate 0,format 0, channels 3, flags 0

01-01 00:34:39.428   212  3957 W NuPlayerRenderer: openAudioSink: non offloaded open failed status: -19

01-01 00:34:39.428   212  3954 E NuPlayer: received error(0xffffffed) from audio decoder, flushing(0), now shutting down

01-01 00:34:39.429   212  3954 D NuPlayerDriver: notifyListener_l(0xb6056d80), (100, 1, -19)

01-01 00:34:39.429   934   948 E MediaPlayer: error (1, -19)

01-01 00:34:39.429   212  3957 W NuPlayerRenderer: onDrainAudioQueue(): audio sink is not ready

01-01 00:34:39.430   212  3957 W NuPlayerRenderer: onDrainAudioQueue(): audio sink is not ready

01-01 00:34:39.430   212  3957 W NuPlayerRenderer: onDrainAudioQueue(): audio sink is not ready

01-01 00:34:39.437   212  3954 W AMessage: failed to post message as target looper for handler 0 is gone.

01-01 00:34:39.501   212   559 E MetadataRetrieverClient: failed to extract an album art

01-01 00:34:39.576   212   441 E MetadataRetrieverClient: failed to extract an album art

01-01 00:34:39.707   934   934 E MediaPlayer: invoke failed: wrong state 0

01-01 00:34:39.708   934   934 E MediaPlayer: Error (1,-19)

01-01 00:34:39.708   934   934 D MultiPlayer: Error: 1,-19

01-01 00:34:39.804   934   934 I imx6.gralloc: open gpu gralloc module!

01-01 00:34:39.894   510   529 I ActivityManager: Displayed com.android.music/.ArtistAlbumBrowserActivity: +1s157ms (total +1s280ms)

01-01 00:34:39.907   934   934 E MediaPlayer: Error (1,-1010)

01-01 00:34:39.907   934   934 D MultiPlayer: Error: 1,-1010

     二、录音出错:

01-01 00:20:36.528   512   948 I ActivityManager: START u0 {act=android.intent.action.MAIN cat=[android.intent.category.LAUNCHER] flg=0x10200000 cmp=com.android.soundrecorder/.SoundRecorder (has extras)} from uid 10010 on display 0

01-01 00:20:36.627   512   884 I ActivityManager: Start proc 9998:com.android.soundrecorder/u0a48 for activity com.android.soundrecorder/.SoundRecorder

01-01 00:20:36.679  9998  9998 I art     : Late-enabling JIT

01-01 00:20:36.694  9998  9998 I art     : JIT created with code_cache_capacity=2MB compile_threshold=1000

01-01 00:20:36.812  9998  9998 W System  : ClassLoader referenced unknown path: /system/app/SoundRecorder/lib/arm

01-01 00:20:37.060  9998 10012 D OpenGLRenderer: Use EGL_SWAP_BEHAVIOR_PRESERVED: true

01-01 00:20:37.068  9998  9998 I imx6.gralloc: open gpu gralloc module!

01-01 00:20:37.227  9998 10012 I OpenGLRenderer: Initialized EGL, version 1.4

01-01 00:20:37.250   205   295 E BufferQueueProducer: [com.android.soundrecorder/com.android.soundrecorder.SoundRecorder] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

01-01 00:20:37.486   512   540 I ActivityManager: Displayed com.android.soundrecorder/.SoundRecorder: +888ms

01-01 00:20:53.653   512   884 I MediaFocusControl:  AudioFocus  requestAudioFocus() from android.media.AudioManager@bae2366 req=1flags=0x0

01-01 00:20:53.719   210   458 E AudioSystem: AudioSystem::getInputBufferSize failed sampleRate 8000 format 0x1 channelMask 10

01-01 00:20:53.719   210   458 E AudioRecord: AudioSystem could not query the input buffer size for sampleRate 8000, format 0x1, channelMask 0x10; status -22

01-01 00:20:53.719   210   458 E StagefrightRecorder: audio source is not initialized

01-01 00:20:53.719  9998  9998 E MediaRecorder: start failed: -2147483648

01-01 00:20:53.985   205   233 E BufferQueueProducer: [com.android.soundrecorder/com.android.soundrecorder.SoundRecorder] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

01-01 00:20:56.168   512   948 W InputMethodManagerService: Window already focused, ignoring focus gain of: com.android.internal.view.IInputMethodClient$Stub$Proxy@3d00f09 attribute=null, token = android.os.BinderProxy@ab205a4

audio source is not initialized01-01 00:22:20.928   512   534 I UsageStatsService: User[0] Flushing usage stats to disk

01-01 00:31:00.029   512   535 I ProcessStatsService: Prepared write state in 12ms

      注:用tinyplay 播放wav 和 tinycap 录音都是正常的.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
5,727件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

1.
 The following is Summary Page link to download Android software 
from NXP Web :

 

Android OS for i.MX Applications Processors|NXP 

2.

  NXP is offering additional packages to extend Android core functionality.
These packages will be available to approved customers and will not be generally
available on NXP.com.

 

There are two packages available:

 

  Extended Multimedia Feature Package

  Wi-Fi Display Sink Feature Package

 

 

The source code package will be provided “as-is” with no support and will be

made available to approved customers via an extranet site.

 

The customer will have options to purchase support or customization services

from NXP.

 

For more information, please create request

https://community.nxp.com/docs/DOC-329745 

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,718件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi talent

had you installed nxp enhanced codecs included in

android_M6.0.1_1.0.0_omxplayer_source.tar.gz software package.

It is described in attached document, procedure for its obtaining

in Release Notes sect.6 Extended Feature Packages

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

5,718件の閲覧回数
leavs
Contributor IV

Do you know where to download the android_M6.0.1_1.0.0_omxplayer_source.tar.gz software package?

0 件の賞賛
返信
5,728件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

1.
 The following is Summary Page link to download Android software 
from NXP Web :

 

Android OS for i.MX Applications Processors|NXP 

2.

  NXP is offering additional packages to extend Android core functionality.
These packages will be available to approved customers and will not be generally
available on NXP.com.

 

There are two packages available:

 

  Extended Multimedia Feature Package

  Wi-Fi Display Sink Feature Package

 

 

The source code package will be provided “as-is” with no support and will be

made available to approved customers via an extranet site.

 

The customer will have options to purchase support or customization services

from NXP.

 

For more information, please create request

https://community.nxp.com/docs/DOC-329745 

Regards,

Yuri.

0 件の賞賛
返信