about ADC sampling clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about ADC sampling clock

ソリューションへジャンプ
2,171件の閲覧回数
goto11
Contributor III

hello,Community

Can I change the ADC sampling clock during operation?
Are there any precautions when making changes?

best regards

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
2,040件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

for clock usage one can look at Figure 14-2. Timing

i.MX 7Dual Applications Processor Reference Manual

Seems it is possible to change clock during operation,

valid data will be on next conversion cycle.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,041件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

for clock usage one can look at Figure 14-2. Timing

i.MX 7Dual Applications Processor Reference Manual

Seems it is possible to change clock during operation,

valid data will be on next conversion cycle.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,040件の閲覧回数
goto11
Contributor III

hello,

Table 93. Recommended operating conditions for 12-bit ADC in .MX 7 Dual Family of Applications Processors Datasheet
Is it OK to make the RIEXT value larger than 250Ω (for example, from several kΩ to dozens of kΩ) when FCLK and FSOC are operated at close Min values?

What kind of problems will occur if the resistance value is increased?

best regards

Goto

0 件の賞賛
返信
2,040件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

for new questions recommended to create new thread.

Best regards
igor

0 件の賞賛
返信