Wrong Qt-Rendering with platform EGLFS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wrong Qt-Rendering with platform EGLFS

ソリューションへジャンプ
9,660件の閲覧回数
michaelwiesent
Contributor II

I have exactly the same problem as in this thread EGLFS ugly rendering. .

In my case i have a display with 800x480 pixel. EGL renders obviously 1000x480 pixel. The 200 pixel are shifted like in the picture below but when i change the parameter bits_per_pixel from 24 to 32 bit (/sys/class/graphics/fb0/bits_per_pixel) the shift will not be visible on the left side. I will simply not be shown anymore because of the end of the display. The rendering failure still exists.

Which init file do jamesbone mean and where can i find this file?

Here are some pictures from my side to give you a better felling what is happening to my system:

Picture 1: this picture shows the effect like above with visible shift

Picture 2: here we can see the same effect but the pixel depth is changed from 24 to 32 bit

Picture 3: this picture shows the output, when i start the example with linuxfb (but in our project we can´t use linuxfb because we use opengl es 2)

IMAG0390_.jpgIMAG0392_.jpgIMAG0391_.jpg

PS: it seems that the eglfs is not interested in the environment variables mentioned here: Qt for Embedded Linux | Qt 5.4

I tested some possible settings but there is no effect to the output. We use Qt 5.3.2 built with yocto in our application.

Also fbset 800 480 800 480 24 only have a effect on the color depth.

Would be perfect if anyone can give some support to me or have some ideas.

Michael

1 解決策
7,247件の閲覧回数
michaelwiesent
Contributor II

Have some great news i want to share. After some searching i found this link

iMX6QD How to Add 24-bit LVDS Support in Android

Here is exactly described how to solve my problem. I have to change the boot parameter. Here is the important part

... if=RGB24,fbpix=RGB32

These parameters describe that the display need RGB24 while the framebuffer holds data with RGB32. After this change it works perfect. Therefore I don´t have to change the EGLFS platform.

Hope i can help somebody else with this information.

元の投稿で解決策を見る

4 返答(返信)
7,247件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

It seems that you have settings incorrect of the  EGL native Window, so in your init function of your application you need to check  EGLQuerySurface. To provide the width and height of EGL.

/*get width and height from egl*/ 
        eglQuerySurface(egldisplay, eglsurface, EGL_WIDTH, &w); 
        eglQuerySurface(egldisplay, eglsurface, EGL_HEIGHT, &h); 
       

0 件の賞賛
返信
7,247件の閲覧回数
michaelwiesent
Contributor II

Thanks for your response.

I don´t exactly know where to set this settings. In the pictures above i tried to use the standard examples from Qt. It´s the example under examples/widgets/animation/animatedtiles. Therefore I don´t think, that I have to change the code for this examples. It has to work.

I also invested some time in getting into the platform coding and the framebuffer. After this i have a guess but don´t know how or where to fix it. When linuxfb is used there are only the RGB values in the framebuffer. It looks like this

R G B R G B R G B ...

When I use the platform eglfs it seems that there is the color format RGBA so it looks like this

R G B A R G B A R G B A ...

The alpha channel has always the value 0xFF. I checked this with hexdump.

I think that the driver (should be vivante) which is interpreting this data do not know about this RGBA format und interpet it like a RGB format. I tried to set the boot parameters to RGBA32 or RGBA8888 but there was no change. The result could be the following:

framebuffer                              R G B A R G B A R G B A

graphic driver interpretation     R G B R G B R G B R G B

This could be the reason why the image is around 200px larger. The basic width is 800px.

I´m able to cross compile the libqeglfs.so. Therefore I added some debugging information for a better understanding how this plugin works. So I can change anything of this plugin. Can anyone tell me where I can set the color width so that only RGB is set to the framebuffer?

UPDATE:
I think i have to change the configuration of the attribute EGL_BUFFER_SIZE or EGL_NATIVE_VISUAL_TYPE from 32 to 24. Where can i do that?

0 件の賞賛
返信
7,248件の閲覧回数
michaelwiesent
Contributor II

Have some great news i want to share. After some searching i found this link

iMX6QD How to Add 24-bit LVDS Support in Android

Here is exactly described how to solve my problem. I have to change the boot parameter. Here is the important part

... if=RGB24,fbpix=RGB32

These parameters describe that the display need RGB24 while the framebuffer holds data with RGB32. After this change it works perfect. Therefore I don´t have to change the EGLFS platform.

Hope i can help somebody else with this information.

7,247件の閲覧回数
hardyb
Contributor III

Thank you for following up. We were addressing this issue on a Wandboard Solo and your fix in the uboot arguments got it for us.

0 件の賞賛
返信