What is the maximum SPI slave devices supported by SPI controller in i.mx8MM?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the maximum SPI slave devices supported by SPI controller in i.mx8MM?

989 次查看
richard_hu
Senior Contributor I

Hi, Sir:

We have a require to enable 8 SPI slave devices on ECSPI2 of i.mx8MM.(using GPIO chip selects)

But we see the description in i.mx8mm TRM denotes the SPI controller supports 4 chip selects for  maximum.

screenshot_1_1632463733.png

 

If we use GPIO chip selects instead of native chip select, does it still limit to four SPI devices?

Or it can support more than four SPI devices?

 

Thanks~!

BR,

 

Richard 

 

 

0 项奖励
回复
1 回复

977 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Richard

 

>If we use GPIO chip selects instead of native chip select, does it still limit to four SPI devices?

 

no, in case of GPIO chip selects it is not limited.

 

Best regards
igor

0 项奖励
回复