What is the maximum SPI slave devices supported by SPI controller in i.mx8MM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the maximum SPI slave devices supported by SPI controller in i.mx8MM?

985 Views
richard_hu
Senior Contributor I

Hi, Sir:

We have a require to enable 8 SPI slave devices on ECSPI2 of i.mx8MM.(using GPIO chip selects)

But we see the description in i.mx8mm TRM denotes the SPI controller supports 4 chip selects for  maximum.

screenshot_1_1632463733.png

 

If we use GPIO chip selects instead of native chip select, does it still limit to four SPI devices?

Or it can support more than four SPI devices?

 

Thanks~!

BR,

 

Richard 

 

 

0 Kudos
Reply
1 Reply

973 Views
igorpadykov
NXP Employee
NXP Employee

Hi Richard

 

>If we use GPIO chip selects instead of native chip select, does it still limit to four SPI devices?

 

no, in case of GPIO chip selects it is not limited.

 

Best regards
igor

0 Kudos
Reply