Flexcan data transfer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexcan data transfer

2,245 Views
Anushree_Shetty
Contributor I

I am using imx6ull processor, it is taking 2 and half seconds to transfer 384 frames at a bitrate of 500kbps. Is there any way to transfer 384 data frames within a second?

0 Kudos
Reply
3 Replies

2,236 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anushree

 

> Is there any way to transfer 384 data frames within a second?

 

in general, one can try to increase bitrate x2 or decrease frame size 1/2.

 

Best regards
igor

0 Kudos
Reply

2,228 Views
Anushree_Shetty
Contributor I

Hi igor,

I want to increase the speed for same bitrate and frame size. Is there any option other than increasing the bitrate and decreasing frame size. 

0 Kudos
Reply

2,217 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anushree

 

in such case you should analyze where delays (if any) between frames happen,
For example remove other running applications, use  MMDC Profiling Tool
0 Kudos
Reply