What is the max. spi clk of imx6 solo for spi nor flash boot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the max. spi clk of imx6 solo for spi nor flash boot?

ソリューションへジャンプ
1,674件の閲覧回数
翔李
Contributor IV

HI

  On imx6 solo,My board boot from spi nor flash 32MB in standard or dual operation and solo not support quad spi.

  what the max. clk freq. of solo to boot from spi nor flash? Is it 60MHZ?And the flash is 104MHZ or 208MHZ for standard or dual spi.So,solo's spi clk is lower to spi nor flash?Pity.

  My flash isW25Q256FVEIG,winbond 32MBYTE SPI NOR FLASH.

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

0 件の賞賛
返信
1 解決策
1,359件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  please look at the following Q&A: What is i.Mx6 ECSPI max frequency? 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

元の投稿で解決策を見る

2 返答(返信)
1,360件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  please look at the following Q&A: What is i.Mx6 ECSPI max frequency? 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

1,359件の閲覧回数
翔李
Contributor IV

From your link,It is only 60mhz for spi nor flash clk.

Thanks.

0 件の賞賛
返信