Hello,
I want to interface parallel NOR flash (256KB*16) with IMXRT1062 but this processor have same port pins for address and data bus. So, I find that ADV#. What is use of this ADV# pin?
I have found this notes for SRAM. Is it same applicable for NOR flash also?
ADV# pin enables Address Path (ADQ=Address Buffer) by asserting ADV# input Low. When ADV# is High, Data Path is enabled (ADQ=I/O Buffer).
解決済! 解決策の投稿を見る。
From the SEMC side, the data and address pins will be on MUX mode so it is not possible to have dedicated address/data pins for NOR flash. The communication will look like this:
Regarding using an external component to separate these signals. It looks viable however I cannot confirm if it is your adequate solution since it was not tested on our side.
Best regards,
Omar
Please reply me!
Yes, the use of ADV on nor flash is similar to the SRAM.
Best regards,
Omar
Ok, Thanks for help.
Please tell me one more thing.
How can I interface parallel NOR flash for separate address bus and data bus? Can we interface directly?
If I interface same terminal of imxrt1062 with NOR flash address and data pins then command will be transfered on both bus of parallel NOR flash.
I have attached one image.
From the SEMC side, the data and address pins will be on MUX mode so it is not possible to have dedicated address/data pins for NOR flash. The communication will look like this:
Regarding using an external component to separate these signals. It looks viable however I cannot confirm if it is your adequate solution since it was not tested on our side.
Best regards,
Omar
Ok thanks