USB config of imx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB config of imx

3,231 Views
pt
Senior Contributor I

Hi all,

evaluation kit: MCIMX28EVK

Linux kernel version:linux 2.6.35 (customized for imx28)

boots up finely. But it doesn't recognize the usb keyboard.

Do I have to set any config of USB?

Regards

pt

Labels (2)
Tags (2)
0 Kudos
Reply
2 Replies

2,961 Views
jamesbone
NXP TechSupport
NXP TechSupport

Can you please share a DMESG to show all the modules that you have already mounted?,  You need to have FSL-EHCI in order to have HID Usb class. In the device.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,958 Views
pt
Senior Contributor I

The error was corrected. It detects the keyboard .(enabled the local echo settings of minicom).

But now the problem I am facing is "login as root".

I am not able to login as root.

0 Kudos
Reply