USB config of imx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB config of imx

3,232 次查看
pt
Senior Contributor I

Hi all,

evaluation kit: MCIMX28EVK

Linux kernel version:linux 2.6.35 (customized for imx28)

boots up finely. But it doesn't recognize the usb keyboard.

Do I have to set any config of USB?

Regards

pt

标签 (2)
标记 (2)
0 项奖励
回复
2 回复数

2,962 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Can you please share a DMESG to show all the modules that you have already mounted?,  You need to have FSL-EHCI in order to have HID Usb class. In the device.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,959 次查看
pt
Senior Contributor I

The error was corrected. It detects the keyboard .(enabled the local echo settings of minicom).

But now the problem I am facing is "login as root".

I am not able to login as root.

0 项奖励
回复