USB config of imx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB config of imx

3,288件の閲覧回数
pt
Senior Contributor I

Hi all,

evaluation kit: MCIMX28EVK

Linux kernel version:linux 2.6.35 (customized for imx28)

boots up finely. But it doesn't recognize the usb keyboard.

Do I have to set any config of USB?

Regards

pt

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

3,018件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Can you please share a DMESG to show all the modules that you have already mounted?,  You need to have FSL-EHCI in order to have HID Usb class. In the device.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,015件の閲覧回数
pt
Senior Contributor I

The error was corrected. It detects the keyboard .(enabled the local echo settings of minicom).

But now the problem I am facing is "login as root".

I am not able to login as root.

0 件の賞賛
返信