The gpio_button abnomal for imx6solo use the linux compiled by imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The gpio_button abnomal for imx6solo use the linux compiled by imx6q

跳至解决方案
1,643 次查看
fdact
Contributor I

Hi,

     I use imx6s porting linux of imx6q, and display is normal. But the gipo_button and i2c can't work , and them are low level, but the same software works normally on imx6q, and all of them are high level.

     The specification of the imx6solo is MCIMX6S6AVM08AC.

Thanks.

标签 (3)
0 项奖励
回复
1 解答
1,558 次查看
jimmychan
NXP TechSupport
NXP TechSupport

i.mx6dl and i.mx6s are the same code.

linux 3.0.35 is quite old. I would suggest you to use the newer bsp.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,558 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Which BSP are you using?

Do you use the IOMUX setting for i.MX6S?

0 项奖励
回复
1,558 次查看
fdact
Contributor I

Hi,

     The BSP is linux3.0.35 and uboot200908. Imx6sl* is the code of imx6sololite. Imx6solo has no separate code branch in linux. Isn't it the same code as imx6q?

    

Thanks.

0 项奖励
回复
1,559 次查看
jimmychan
NXP TechSupport
NXP TechSupport

i.mx6dl and i.mx6s are the same code.

linux 3.0.35 is quite old. I would suggest you to use the newer bsp.

0 项奖励
回复