Hi,
I use imx6s porting linux of imx6q, and display is normal. But the gipo_button and i2c can't work , and them are low level, but the same software works normally on imx6q, and all of them are high level.
The specification of the imx6solo is MCIMX6S6AVM08AC.
Thanks.
Solved! Go to Solution.
i.mx6dl and i.mx6s are the same code.
linux 3.0.35 is quite old. I would suggest you to use the newer bsp.
Which BSP are you using?
Do you use the IOMUX setting for i.MX6S?
Hi,
The BSP is linux3.0.35 and uboot200908. Imx6sl* is the code of imx6sololite. Imx6solo has no separate code branch in linux. Isn't it the same code as imx6q?
Thanks.
i.mx6dl and i.mx6s are the same code.
linux 3.0.35 is quite old. I would suggest you to use the newer bsp.