The gpio_button abnomal for imx6solo use the linux compiled by imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The gpio_button abnomal for imx6solo use the linux compiled by imx6q

ソリューションへジャンプ
1,808件の閲覧回数
fdact
Contributor I

Hi,

     I use imx6s porting linux of imx6q, and display is normal. But the gipo_button and i2c can't work , and them are low level, but the same software works normally on imx6q, and all of them are high level.

     The specification of the imx6solo is MCIMX6S6AVM08AC.

Thanks.

ラベル(3)
0 件の賞賛
返信
1 解決策
1,723件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

i.mx6dl and i.mx6s are the same code.

linux 3.0.35 is quite old. I would suggest you to use the newer bsp.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,723件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which BSP are you using?

Do you use the IOMUX setting for i.MX6S?

0 件の賞賛
返信
1,723件の閲覧回数
fdact
Contributor I

Hi,

     The BSP is linux3.0.35 and uboot200908. Imx6sl* is the code of imx6sololite. Imx6solo has no separate code branch in linux. Isn't it the same code as imx6q?

    

Thanks.

0 件の賞賛
返信
1,724件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

i.mx6dl and i.mx6s are the same code.

linux 3.0.35 is quite old. I would suggest you to use the newer bsp.

0 件の賞賛
返信