Simple Ram interface to imx6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simple Ram interface to imx6Q

ソリューションへジャンプ
2,004件の閲覧回数
nishad_kamdar
Contributor IV

Hi,

I was going through some files in the L3.0.35_4.1.0 for accessing the memory connected to the EIM bus as a simple RAM.

I came across mtdram.c and map_ram.c

Can anyone explain their significance to me and tell me how i can use them to access an SRAM connected to an MX6q on the EIM bus with a chip select

regards,

nishad

ラベル(1)
0 件の賞賛
返信
1 解決策
1,735件の閲覧回数
Yuri
NXP Employee
NXP Employee

As mentioned in

SRAM support on EIM bus existing drivers

it makes sense to reuse the WEIM driver, included in i.MX6 Sabre AI design.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,736件の閲覧回数
Yuri
NXP Employee
NXP Employee

As mentioned in

SRAM support on EIM bus existing drivers

it makes sense to reuse the WEIM driver, included in i.MX6 Sabre AI design.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信