Simple Ram interface to imx6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Simple Ram interface to imx6Q

跳至解决方案
2,008 次查看
nishad_kamdar
Contributor IV

Hi,

I was going through some files in the L3.0.35_4.1.0 for accessing the memory connected to the EIM bus as a simple RAM.

I came across mtdram.c and map_ram.c

Can anyone explain their significance to me and tell me how i can use them to access an SRAM connected to an MX6q on the EIM bus with a chip select

regards,

nishad

标签 (1)
0 项奖励
回复
1 解答
1,739 次查看
Yuri
NXP Employee
NXP Employee

As mentioned in

SRAM support on EIM bus existing drivers

it makes sense to reuse the WEIM driver, included in i.MX6 Sabre AI design.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,740 次查看
Yuri
NXP Employee
NXP Employee

As mentioned in

SRAM support on EIM bus existing drivers

it makes sense to reuse the WEIM driver, included in i.MX6 Sabre AI design.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复