Silicon Revision on iMX8QXP Dev Kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Silicon Revision on iMX8QXP Dev Kit

2,845件の閲覧回数
rlumo
Contributor II

I would like to know what is the Silicon Revision on my iMX8QXP Dev Kit.

I have the following stickers on the back of my dev kit:

S/N VV 19420385

SCH-29683 REV C2

700-29683 REV C2

TDA 7239

0 件の賞賛
返信
3 返答(返信)

2,793件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

You may try 2 ways to identify the silicon revision for the chip:

 

  • Use "misc_get_control" with "SC_R_SYSTEM" and "SC_C_ID" to get the REV info.
  • Check the last letter of the part number, which indicates the silicon reversion.

 

In your case it may be easier to identify using the second method, simx8qx6avlf1bb -> B0 chip

 

Hope this helps,

Best regards,

Aldo.

0 件の賞賛
返信

2,765件の閲覧回数
darsh_dev
Contributor V
0 件の賞賛
返信

2,793件の閲覧回数
rlumo
Contributor II

Also these are the markings on the chip.

simx8qx6avlf1bb
sbae 1928
1N95W
korea mbaesbc
0 件の賞賛
返信