Question, i.MX6Q SATA link-down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6Q SATA link-down

Jump to solution
3,684 Views
Aemj
Contributor IV

Dear team,

I would like to ask about SATA initialization of i.MX6Q.

My customer is facing the issue that SATA link-down could be seen on the customer’s i.MX6Q board.

In the customer’s investigation, they found the COMRESET does not be sent from i.MX6 at that time. And after the link-down occur, COMRESET does not be sent even when they execute the following command from linux console.

# cd /unit_tests

# ./memtool -32 02200004=80000003

# ./memtool -32 02200118=7

We already read the ERR003761, but the errata is that when COMRESET is sent it sometimes send only five bursts. From the fact that nothing is sent from i.MX6, they think the issue on the customer’s lab is not related to the erratum.

Do you have any ideas about the cause of this issue?

BTW, the customer is using your LinuxBSP L3.0.35_4.1.0.

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Solution
3,022 Views
jamesbone
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
4 Replies
3,023 Views
jamesbone
NXP TechSupport
NXP TechSupport

It may be clock issue. Can you please try this patch?

  

  0001-ENGR00296249-sata-cr-rst-workaround-sata-phy-link-is.patch.zip

0 Kudos
Reply
3,022 Views
Aemj
Contributor IV

Hi jamesbone,

I have downloaded the patch from other discussion.

[Linux][i.mx6] When I boot form emmc, sometime failed to mount sata in kernel.

Could you explain what the patch is for?

What is solved by the patch?

BR,

Miyamoto

0 Kudos
Reply
3,022 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello ,

The patch fix some clock issue of the SATA port that does not allow to have a complete link of the device with the disk

0 Kudos
Reply
3,022 Views
Aemj
Contributor IV

Hi Jamesbone,

I cannot dwonload the path file from the link you added in your comment.

Could you check the link you added in your comment?

BR,

Miyamoto

0 Kudos
Reply