Raw RGB (Bayer) 10-bit on i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Raw RGB (Bayer) 10-bit on i.MX6DL

2,412 Views
antonpavlov
Contributor I

I am considering to use i.MX6DL (Yocto Linux kernel 3.10) with AR0330 camera sensor connected via MIPI interface.

The camera operation mode is following:

lanes = 2-lanes mipi 

pixel format = Raw RGB (Bayer RGGB) 10-bit

Fserial = 480Mhz

PixelRate = 98 Mpixel/s

Does anyone know if i.MX6DL is able to handle this configuration?

Labels (3)
Tags (2)
0 Kudos
2 Replies

701 Views
igorpadykov
NXP Employee
NXP Employee

HI Anton

I think it may be supported, MIPI CSI-2 main characteristics are given on p.68

presentation below

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

701 Views
antonpavlov
Contributor I

Hi Igor,

Thanks for your prompt answer.

Special thanks for the presentation which was extremely helpful!

In fact, based on the reference manual and on the presentation, there is a possibility to implement the operation mode mentioned in my question.

Thanks again and best regards,

Anton

0 Kudos