Hello,
OCRAM_PXP mainly is used, when the PXP and LCDIF support a mode where
the internal RAM serves as frame buffer to minimize external memory bandwidth.
Also, You may look at Figure 13-87 (PXP Architecture) of i.MX7D RM, showing Internal
RAM using. So, it is not recommended to use OCRAM_PXP, when the PXP is working.
It is possible to implement data path from CSI camera to LCD without PXP.
Also, please look at About OCRAM_S in i.MX7Solo
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------