Hello,
from the linked below Community thread :
The GPIO buffer load capacity is not specified in units of current. It is specified in terms of buffer
drive strength or output impedance; refer to the Section "GPIO Output Buffer Impedance" of the i.MX6
Data Sheet(s).
what is value of GPIO source/sink current per pin on i.MX6?
IBIS models may be used to estimate current.
https://community.nxp.com/message/395489
I looked at i.MX6Q IBIS file - 3 mA may be provided by i.MX6, assuming proper
GPIO drive strength and external impedance are selected.
Also, the total load current and power dissipation should be taken into account when calculating the
GPIO power budget.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------