Re: mx6ul kernel secure boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: mx6ul kernel secure boot

1,468件の閲覧回数
giuliodominutti
Contributor III

I have one more question about this subject. At the end I use fuse prog to save SRK hash values in OTP and all is working as supposed, with no hab events.
After that I also use encryption and again  all is working fine and properly.

The last step was also sign the kernel image with CSF tool, and again also this part was easy and the check returns no hab events found, but now I'm asking if i can also encrypt kernel image using the CSF tools. (this is not specified anywhere)

Thanks

1 返信

1,396件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Sorry, but the information you are requesting is treated as confidential info at this time and

requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with

you in public anyway, this requires to be handled as a Service Request (SR).

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信