Pin processing when USB interface is not used of i.MX6Solo.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Pin processing when USB interface is not used of i.MX6Solo.

跳至解决方案
1,601 次查看
takashitakahash
Contributor III

Hi community.

Our customer has question below.

Please tell me about pin processing when not using USB analog interface.
,
IMX6DQ6SDLHDG does not describe the processing of F9 (VDDUSB_CAP), V5 (USB_OTG_PWR), T4 (USB_OTG_ID).

Could you tell me how to handle the terminals?
As USB is not used, is itcorrect with GND short?

Thank you.

Best Regards.

T.Takahashi

标签 (1)
0 项奖励
回复
1 解答
1,390 次查看
Yuri
NXP Employee
NXP Employee

Hello

1.
VDDUSB_CAP requires capacitor if the internal regulator is used, otherwise -may be left float.

 

2.

  USB_OTG_PWR, USB_OTG_ID may be left float, assuming default GPIO mode of corresponding pins.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,391 次查看
Yuri
NXP Employee
NXP Employee

Hello

1.
VDDUSB_CAP requires capacitor if the internal regulator is used, otherwise -may be left float.

 

2.

  USB_OTG_PWR, USB_OTG_ID may be left float, assuming default GPIO mode of corresponding pins.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 项奖励
回复