Pin processing when USB interface is not used of i.MX6Solo.

cancel
Showing results for 
Search instead for 
Did you mean: 

Pin processing when USB interface is not used of i.MX6Solo.

Jump to solution
456 Views
takashitakahash
Contributor III

Hi community.

Our customer has question below.

Please tell me about pin processing when not using USB analog interface.
,
IMX6DQ6SDLHDG does not describe the processing of F9 (VDDUSB_CAP), V5 (USB_OTG_PWR), T4 (USB_OTG_ID).

Could you tell me how to handle the terminals?
As USB is not used, is itcorrect with GND short?

Thank you.

Best Regards.

T.Takahashi

Labels (1)
0 Kudos
1 Solution
245 Views
Yuri
NXP TechSupport
NXP TechSupport

Hello

1.
VDDUSB_CAP requires capacitor if the internal regulator is used, otherwise -may be left float.

 

2.

  USB_OTG_PWR, USB_OTG_ID may be left float, assuming default GPIO mode of corresponding pins.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

View solution in original post

0 Kudos
1 Reply
246 Views
Yuri
NXP TechSupport
NXP TechSupport

Hello

1.
VDDUSB_CAP requires capacitor if the internal regulator is used, otherwise -may be left float.

 

2.

  USB_OTG_PWR, USB_OTG_ID may be left float, assuming default GPIO mode of corresponding pins.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

View solution in original post

0 Kudos