OpenWRT Source and Buildroot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenWRT Source and Buildroot

7,062件の閲覧回数
arvinlim
Contributor II

I'm working on a project to develop a gateway designed with iMX6.Ul soc, would you please share me the codes and the buildroot referenced by the topic https://community.nxp.com/docs/DOC-331175   .

I would appreciate it very much.edk

ラベル(2)
タグ(1)
0 件の賞賛
返信
7 返答(返信)

5,861件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

All the i.MX6 variants (i.MX6UL included) are supported by mainline Buildroot:

buildroot - Buildroot: Making Embedded Linux easy 

So you only need to download the latest stable release and you're good to go.

Buildroot - Making Embedded Linux Easy 

Regards,

Gary

0 件の賞賛
返信

5,861件の閲覧回数
arvinlim
Contributor II

Hi, Gary,

Sorry, Maybe I'm not clear enough.

When I talk about 'Buildroot',I really mean the OpenWRT building enviroment.

So, Is there anywhere to download the iMX6.Ul's OpenWRT building enviroment?

Regards,

Arvin

0 件の賞賛
返信

5,861件の閲覧回数
gary_bisson
Senior Contributor III

Hi Arvin,

Ok, then discard my comment, Buildroot and OpenWRT are completely different now.

As for OpenWRT, the mainline version doesn't seem to support this CPU.

openwrt/target/linux/imx6 at master · openwrt/openwrt · GitHub 

Regards,

Gary

0 件の賞賛
返信

5,861件の閲覧回数
arvinlim
Contributor II

Hi Gary,

I'm so sorry for referencing the wrong URL address, now I have updated it.

Please help. Thanks very much.

Regards,

Arvin

0 件の賞賛
返信

5,861件の閲覧回数
gary_bisson
Senior Contributor III

Hi Arvin,

Well I'm no NXP employee so I can't help you with the sources of that demo.

I only tried to help because I maintain i.MX6 support in Buildroot.

Regarding OpenWRT, I guess you just need to update the kernel "recipe" to use the latest 4.1.15 one from NXP. But I won't be able to help you any further, good luck!

Regards,

Gary

5,861件の閲覧回数
arvinlim
Contributor II

Hi, Gary,

Sorry for my mistake.Thanks all the same.

Regards,

Arvin

0 件の賞賛
返信

5,861件の閲覧回数
arvinlim
Contributor II

Hi Gary,

Yes, I have checked the OpenWRT github repo, and found that doesn't support this CPU.

When I search more from internet,  Google lead me to  this content, https://community.nxp.com/docs/DOC-331175 ,

It seems that your guys has ported this CPU to OpenWRT, so that's why I'm seeking help in community.

Regards,

Arvin

0 件の賞賛
返信