Reg:Imx6 MIPI 2 lane interface with MIPI 4 lane LCD and LVDS to MIPI 4 lane Conveter Chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reg:Imx6 MIPI 2 lane interface with MIPI 4 lane LCD and LVDS to MIPI 4 lane Conveter Chip

6,165 Views
sathiyandurai
Contributor II

Hello,

We are using IMx6 Dual Core CPU and 5.2inch FHD LCD in our Design. We have some clarfication regarding between LCD and IMX6 interface below please clarify us

Query 1:

IMx6 Dual CPU support MIPI 2 Lane Interface and our LCD support MIPI 4 Lane Interface, How i will Interface both (2Lane with 4 Lane)?

Query 2:

Whether any one know LVDS or HDMI to MIPI 4 Lane Converter Chip?

Host Interface: LVDS or HDMI

LCD Interface: MIPI 4 Lane

Best Regards

Sathiyan. D

2 Replies

2,309 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Sathiyan,

>>Query 1:

The max speed of MIPI DSI port on iMX6 is 2Gbps, and support XVGA/SVGA/WVGA/VGA/CIF/QCIF,QVGA/QQVGA resolution. For your LCD, you should check if it can work at 2-lane mode, I think it can.

>>Query 2:

LVDS to MIPI :DS90C387/DS90C388

HDMI to MIPI: TC358779XBG

Just provide 2 examples, you can evaluate them, or look for other chips!

Have a nice day!

Best regards,

Weidong

0 Kudos

2,309 Views
robertoluo
Contributor II

HDMI to MIPI EDP LVDS TTL RGB Convertor RK3288 for 2K 4K Dual Multi Touch LCD OLED Displays China

www.confuindustries.com
Specializing in HDMI to MIPI DSI EDP LVDS TTL RGB Interface Adapters RK3288 Dual Multi Displays. Applied for LCD OLED Display (2K 4K): VR HMD, Raspberry Pi,3D Printer, PC,TV, Car Displays, POS,PLC, Advertising Machine.
Confu HDMI TO MIPI DSI Tested Models (2K 4K, Singal / Dual Screens, Touch Function)
Brand Model Display Size Resolution(S) Resolution(Dual)
SHARP LS029B3SX02 LCD 2.89 1440*1440 2880*1440 70Hz  
SHARP LS055T1SX01 LCD 5 1080*1920 NA 50-60Hz  
SHARP LS055R1SX03 LCD 5.5 1440*2560 NA 50-60Hz  
SHARP LS055R1SX04 LCD 5.5 1440*2560 NA 50-60Hz  
SHARP LS060R1SX01 LCD 6 1440*2560 NA 50-60Hz  
SHARP LS079L1SX02F LCD 7.9 1536*2048 NA 50-60Hz  
JDI ACX450AKN-7 LCD 5 1080*1920 NA 50-60Hz  
JDI ACX465AKM-7 LCD 5.9 1080*1920 NA 50-60Hz  
JDI LPM055A138A LCD 5.5 1440*2560 NA 50-60Hz  
JDI LPM055A184A LCD 5.5 1440*2560 NA 50-60Hz  
JDI LT070ME05000 LCD 7 1200*1920 NA 50-60Hz  
JDI TFTMD089030 LCD 8.9 2560*1600 NA 50-60Hz  
AUO H546DLB01.2 OLED 5.5 1080*1920 NA 50-60Hz  
AUO H381DLN01.2 OLED 3.81 1080*1200 2160*1200 90Hz  
Everdisplay E295FMM1 OLED 2.95 1080*1200 2160*1200 90Hz  
BOE NA LCD 3.5 1440*1600 2880*1600 60Hz  
Samsung AMS567DJ01 OLED 5.67 1440*2560 NA 60Hz Note4
Sony Z5 4K AMS567DJ01 IPS 5.5 3840*2160 NA 30H