Nitrogen8M_Plus_SOM Yocto basler daa3840-30mc Image anomaly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nitrogen8M_Plus_SOM Yocto basler daa3840-30mc Image anomaly

619 Views
kylin_wan
Contributor I

issue Description: Nitrogen8M_Plus_SOM development board + LVDS1280X800 screen running Yocto system, connected to a Basler daa3840-30mc camera. GStreamer (GST) executes normally, but nothing (such as objects or faces) is visible in the video. When shaking the camera, changes can be seen in the video, indicating movement.

Debugging Process:

  • Device tree: imx8mp-nitrogen8mp.dts
  • Command:
    GST_DEBUG=4 gst-launch-1.0 -v v4l2src device=/dev/video3 ! video/x-raw,width=1280,height=800,force-aspect-ratio=true ! videoconvert ! waylandsink
  • Attempted to output the video to a file using GST, and the image seen in the file matches what is shown on the LVDSscreen.

Attachments: Log, video

   Download link
https://we.tl/t-q0WHZYJic8

0 Kudos
Reply
2 Replies

595 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Maybe someone from @Ezurio can help.

Regards

0 Kudos
Reply

593 Views
kylin_wan
Contributor I
OK,I Will consult.
0 Kudos
Reply