Nitrogen8M_Plus_SOM Yocto basler daa3840-30mc Image anomaly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Nitrogen8M_Plus_SOM Yocto basler daa3840-30mc Image anomaly

623 次查看
kylin_wan
Contributor I

issue Description: Nitrogen8M_Plus_SOM development board + LVDS1280X800 screen running Yocto system, connected to a Basler daa3840-30mc camera. GStreamer (GST) executes normally, but nothing (such as objects or faces) is visible in the video. When shaking the camera, changes can be seen in the video, indicating movement.

Debugging Process:

  • Device tree: imx8mp-nitrogen8mp.dts
  • Command:
    GST_DEBUG=4 gst-launch-1.0 -v v4l2src device=/dev/video3 ! video/x-raw,width=1280,height=800,force-aspect-ratio=true ! videoconvert ! waylandsink
  • Attempted to output the video to a file using GST, and the image seen in the file matches what is shown on the LVDSscreen.

Attachments: Log, video

   Download link
https://we.tl/t-q0WHZYJic8

0 项奖励
回复
2 回复数

599 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Maybe someone from @Ezurio can help.

Regards

0 项奖励
回复

597 次查看
kylin_wan
Contributor I
OK,I Will consult.
0 项奖励
回复