Nitrogen8M_Plus_SOM Yocto basler daa3840-30mc Image anomaly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Nitrogen8M_Plus_SOM Yocto basler daa3840-30mc Image anomaly

624件の閲覧回数
kylin_wan
Contributor I

issue Description: Nitrogen8M_Plus_SOM development board + LVDS1280X800 screen running Yocto system, connected to a Basler daa3840-30mc camera. GStreamer (GST) executes normally, but nothing (such as objects or faces) is visible in the video. When shaking the camera, changes can be seen in the video, indicating movement.

Debugging Process:

  • Device tree: imx8mp-nitrogen8mp.dts
  • Command:
    GST_DEBUG=4 gst-launch-1.0 -v v4l2src device=/dev/video3 ! video/x-raw,width=1280,height=800,force-aspect-ratio=true ! videoconvert ! waylandsink
  • Attempted to output the video to a file using GST, and the image seen in the file matches what is shown on the LVDSscreen.

Attachments: Log, video

   Download link
https://we.tl/t-q0WHZYJic8

0 件の賞賛
返信
2 返答(返信)

600件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Maybe someone from @Ezurio can help.

Regards

0 件の賞賛
返信

598件の閲覧回数
kylin_wan
Contributor I
OK,I Will consult.
0 件の賞賛
返信