MfgTool image downloading error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MfgTool image downloading error

ソリューションへジャンプ
2,948件の閲覧回数
xhlow
Contributor II

Hi All,

I just received a MCIMX6ULL-EVK this week. I tried to download image using MfgTool2 with  L4.9.88_2.0.0 iMX6,7 BSP. But it show error message below when I downloading the image.

 
U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1b (May 01 2018 - 15:03:05 -05 00)

CPU: Freescale i.MX6ULL rev1.0 at 396 MHz
Reset cause: POR
Model: Freescale i.MX6 ULL DDR3 ARM2 Board
Board: MX6ULL 14X14 DDR3 ARM2
DRAM: 1 GiB
ERROR: read error from device: bef4a9a8 register: 0x0!
at /home/bamboo/build/4.9.X-2.X/fsl-imx-xwayland/temp_build_dir/build_fsl-imx-xw ayland/tmp/work/imx6ull14x14ddr3arm2-poky-linux-gnueabi/u-boot-imx/2017.03-r0/gi t/drivers/power/pmic/pfuze100.c:46/pfuze100_read()
Not supported, id=11
initcall sequence bffa8920 failed at call 878042d4 (err=-22)
### ERROR ### Please RESET the board ###

Kindly need your help on this?

Thanks.

Regards,

XH Low

ラベル(4)
0 件の賞賛
返信
1 解決策
2,668件の閲覧回数
xhlow
Contributor II

Hi Igor,

We able to download the image. Just double click one of the desired .vbs script to run the mfgtool.

Thanks.

Regards,
XH Low

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,669件の閲覧回数
xhlow
Contributor II

Hi Igor,

We able to download the image. Just double click one of the desired .vbs script to run the mfgtool.

Thanks.

Regards,
XH Low

0 件の賞賛
返信
2,668件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi XH Low

from log it is not MCIMX6ULL-EVK but "MX6ULL 14X14 DDR3 ARM2" and it has

different uboot image:

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,668件の閲覧回数
xhlow
Contributor II

Hi Igor,

May I know where to get this u-boot image? 

Thanks.


Regards,

XH Low

0 件の賞賛
返信
2,668件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信