Mfgtool abnormal exit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mfgtool abnormal exit

1,841件の閲覧回数
mokey
Contributor I

hello:

            Now use the code imx6q Android8.0, download the firmware and tool from the official website, open the Mfgtool tool, power the board, plug in the USB, Mfgtool abnormal exit。

log:

DLL version: 2.7.0
Tuesday, October 16, 2018 10:22:31   Start new logging
ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[01359DD0]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0135A278]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0588E7A0]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0588EB40]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0588F220]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[01358DD0]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0590E850]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0590EB30]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[013594B0]
ModuleID[2] LevelID[10]: Device Manager thread is running
ModuleID[2] LevelID[1]: Can't set m_hStopEvent before it initialized or it already stop
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,734件の閲覧回数
张松源
Contributor III

hi  mokey one,   

have you solve this problem, please tell me the way.  I was using  imx6sl Android8.0.

0 件の賞賛
返信

1,734件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mokey

detailed description of mfg tool usage is provided in Android_Quick_Start_Guide.pdf provided with package,

also one can check if correct package was used and try to test with i.MX6Q Sabre SD reference board:

i.MX 6/7D Series Manufacturing Toolkit for Android O8.0.0_1.0.0 Release

https://www.nxp.com/webapp/Download?colCode=IMX_O8.0.0_1.0.0_TOOL&appType=license&location=null&Pare... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信