MfgTool image downloading error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MfgTool image downloading error

跳至解决方案
2,951 次查看
xhlow
Contributor II

Hi All,

I just received a MCIMX6ULL-EVK this week. I tried to download image using MfgTool2 with  L4.9.88_2.0.0 iMX6,7 BSP. But it show error message below when I downloading the image.

 
U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1b (May 01 2018 - 15:03:05 -05 00)

CPU: Freescale i.MX6ULL rev1.0 at 396 MHz
Reset cause: POR
Model: Freescale i.MX6 ULL DDR3 ARM2 Board
Board: MX6ULL 14X14 DDR3 ARM2
DRAM: 1 GiB
ERROR: read error from device: bef4a9a8 register: 0x0!
at /home/bamboo/build/4.9.X-2.X/fsl-imx-xwayland/temp_build_dir/build_fsl-imx-xw ayland/tmp/work/imx6ull14x14ddr3arm2-poky-linux-gnueabi/u-boot-imx/2017.03-r0/gi t/drivers/power/pmic/pfuze100.c:46/pfuze100_read()
Not supported, id=11
initcall sequence bffa8920 failed at call 878042d4 (err=-22)
### ERROR ### Please RESET the board ###

Kindly need your help on this?

Thanks.

Regards,

XH Low

标签 (4)
0 项奖励
回复
1 解答
2,671 次查看
xhlow
Contributor II

Hi Igor,

We able to download the image. Just double click one of the desired .vbs script to run the mfgtool.

Thanks.

Regards,
XH Low

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,672 次查看
xhlow
Contributor II

Hi Igor,

We able to download the image. Just double click one of the desired .vbs script to run the mfgtool.

Thanks.

Regards,
XH Low

0 项奖励
回复
2,671 次查看
igorpadykov
NXP Employee
NXP Employee

Hi XH Low

from log it is not MCIMX6ULL-EVK but "MX6ULL 14X14 DDR3 ARM2" and it has

different uboot image:

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,671 次查看
xhlow
Contributor II

Hi Igor,

May I know where to get this u-boot image? 

Thanks.


Regards,

XH Low

0 项奖励
回复
2,671 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复