Mcuboot project not shows when importing projects with config tools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mcuboot project not shows when importing projects with config tools

ソリューションへジャンプ
1,003件の閲覧回数
shizj
Contributor III

config tools import projects.PNG

As shown above. I also find the same problem with "lwip_httpscli_ota_enet", "lwip_httpscli_ota_wifi" projects.

Now I have to copy and edit the project‘s setting manually to make it detached. A really boring work. T_T

 

Version Info

SDK: SDK_2_11_1_EVK-MIMXRT1060

config tools: 11.0.0.202201111056

0 件の賞賛
返信
1 解決策
1,000件の閲覧回数
shizj
Contributor III

Sorry a mistake. The reason is when I update the SDK and unzip files with “not over-write existing files” options. So manifest.xml is not update which config tools used to recognize SDK.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,001件の閲覧回数
shizj
Contributor III

Sorry a mistake. The reason is when I update the SDK and unzip files with “not over-write existing files” options. So manifest.xml is not update which config tools used to recognize SDK.

0 件の賞賛
返信