Mcuboot project not shows when importing projects with config tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mcuboot project not shows when importing projects with config tools

Jump to solution
995 Views
shizj
Contributor III

config tools import projects.PNG

As shown above. I also find the same problem with "lwip_httpscli_ota_enet", "lwip_httpscli_ota_wifi" projects.

Now I have to copy and edit the project‘s setting manually to make it detached. A really boring work. T_T

 

Version Info

SDK: SDK_2_11_1_EVK-MIMXRT1060

config tools: 11.0.0.202201111056

0 Kudos
Reply
1 Solution
992 Views
shizj
Contributor III

Sorry a mistake. The reason is when I update the SDK and unzip files with “not over-write existing files” options. So manifest.xml is not update which config tools used to recognize SDK.

View solution in original post

0 Kudos
Reply
1 Reply
993 Views
shizj
Contributor III

Sorry a mistake. The reason is when I update the SDK and unzip files with “not over-write existing files” options. So manifest.xml is not update which config tools used to recognize SDK.

0 Kudos
Reply