Mcuboot project not shows when importing projects with config tools

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Mcuboot project not shows when importing projects with config tools

跳至解决方案
1,054 次查看
shizj
Contributor III

config tools import projects.PNG

As shown above. I also find the same problem with "lwip_httpscli_ota_enet", "lwip_httpscli_ota_wifi" projects.

Now I have to copy and edit the project‘s setting manually to make it detached. A really boring work. T_T

 

Version Info

SDK: SDK_2_11_1_EVK-MIMXRT1060

config tools: 11.0.0.202201111056

0 项奖励
回复
1 解答
1,051 次查看
shizj
Contributor III

Sorry a mistake. The reason is when I update the SDK and unzip files with “not over-write existing files” options. So manifest.xml is not update which config tools used to recognize SDK.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,052 次查看
shizj
Contributor III

Sorry a mistake. The reason is when I update the SDK and unzip files with “not over-write existing files” options. So manifest.xml is not update which config tools used to recognize SDK.

0 项奖励
回复