MMPF0100 POWERON

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,068件の閲覧回数
atillametetured
Contributor V

Greetings,

On the Sabre board for Smart Devices of iMX6, the PMIC power on pin is connected to VSNVS rail and this confuses me. If PWRON pin is configured as level sensitive such that active high turns the device on, how can it turn itself on when is is not yet turned on and there is no voltage on the VSNVS output? Can someone explain? Perhaps I am misinterpreting the situation.

Regards,

Mete

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,747件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

The PMIC VSNVS pin is connected to Li-cel, assuming it is always ON power,

or it is powered first during PMIC Start-up Sequence. Please refer to PMIC

Datasheet about its power up sequence.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,748件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

The PMIC VSNVS pin is connected to Li-cel, assuming it is always ON power,

or it is powered first during PMIC Start-up Sequence. Please refer to PMIC

Datasheet about its power up sequence.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------